• Prihlásiť
  • Prihlásenie

Factory Automation

Print page

Automatica 2018 – 360° Connectivity

What we will show

360° Connectivity. What does it mean? In cooperation with our partners we present exciting trend topics such as robotics in the context of digitization, OEE, maintenance and monitoring/analysis tools for drive and control technology and an overview of our extensive robot portfolio.


Make your production more flexible

At our booth you will learn how digitization can make your production more flexible. The intelligent use of integrated automation platforms opens up new potential for production optimization.

Among other things, all application data from the robotic, drive and control systems of Mitsubishi Electric's automation world and the partner applications are transferred to the higher-level SCADA system MAPS (Mitsubishi Androit Process Suite).

Experience live how data from the production environment is collected and transmitted to MAPS for visualization, monitoring and process analysis and how Mitsubishi Electric's e-F@ctory concept offers a way to develop solutions for direct connection of production to the cloud.


Collaborative robot

While the precision of some collaborative robots may be reduced in comparison with industrial versions, the Mitsubishi Electric model’s performance characteristics mirror those of the company’s industrial autonomous robot range. This means a repeat accuracy of ±0.02 mm, despite the inclusion of sensitive force/torque sensors. Load capacity of the shown robot model is between 5 and 6 kg and reach is between 800 and 1000 mm.

As well as performance, Mitsubishi Electric has also addressed ease of use, with innovative and, to date, unique control and programming options. A touch-screen operator terminal, which can be plugged into the robot, provides an intuitive interface to ‘teach’ the robot its task, without any special programming expertise. The teach functionality includes a ‘direct control’ mode which allows the operator to move the robot from position to position, by hand and with controlled force. Once the set-up is complete, the operator terminal is easily removed to give the robot full freedom of movement.

See the prototype live at our booth


MELFA EasyFeed - Flexible, compact and cost-optimized part feeding

Flexible part feeding in conjunction with robots opens up new possibilities in almost every industry. The cost-optimized and flexible solution for separating and orienting small to large components ensures quality requirements even for sensitive products.

The MELFA EasyFeed solution with our e-F@ctory partner Asyril enables space-saving cells for machine assembly for innovative automation systems.


Come to us

Hall B5, Stand 318

Your way to your free entrance tickets and/or an appointment

KontaktPolia označené s * sú povinné.

Kombinácia z písmen a  číslic Aktualizovať

späť

Dopyty
Kontakt
Informačná základňa
Pomoc